This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

高低压及单端到差分转换



您好,我在电路设计时遇到的问题是:

前面一个模块采用高压10V电源供电,输出方式为单端输出,输出信号范围为5±4V,而后端输入为3.3V电源供电,采用全差分的输入方式,输入范围为1.65V±0.75V。两个模块之间需要一个接口电路,用于实现单端到差分,及电压范围变换的功能,TI有推荐的方案没?谢谢!