Part Number: ADS1299
已经成功读取到了内部测试信号的矩形波,但幅值范围有问题,我设置增益为24,测得的信号单边幅值为0.000018V,正常应该为0.0018V,设置寄存器chnset = 0x61,增益为24,测量内部噪声,八个通道的噪声范围在-0.00089V~-0.00009V,之后又测量了MVDD模式,发现无论设置增益为1还是24,八个通道的输出都是直接达到上限(增益为1时是4.5V,增益为24时是0.1875V),想问下这是什么原因,有什么解决方法。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS1299
已经成功读取到了内部测试信号的矩形波,但幅值范围有问题,我设置增益为24,测得的信号单边幅值为0.000018V,正常应该为0.0018V,设置寄存器chnset = 0x61,增益为24,测量内部噪声,八个通道的噪声范围在-0.00089V~-0.00009V,之后又测量了MVDD模式,发现无论设置增益为1还是24,八个通道的输出都是直接达到上限(增益为1时是4.5V,增益为24时是0.1875V),想问下这是什么原因,有什么解决方法。
您好,
根据“9.6.1.3 CONFIG2”, 内部测试信号幅值只有两种选择,
通过内部测试信号的读取,可帮助理清是否存在通讯问题和配置问题。
这个帖子请参考。
ADS1299:Incorrect Test Signal - Data converters forum - Data converters - TI E2E support forums
您好,
我设置了config2的值为0xD0,算出测试信号幅值在0.0018V,频率是1Hz,但读取的信号幅值是0.000018V,频率没有出现问题。
目前发现VCAP4引脚电压可能有问题,我使用的电源为DVDD = 3.3V、AVDD = +2.5V和AVSS = -2.5V,测得VREFP = 2V,VREFN = -2.5V,VCAP1 = -1.3V,VCAP2 = 3mV,VCAP3 = 4.4V,VCAP4 = 1.4V。其中VCAP4不太符合AVSS+(VREFP +VREFN)/2。
上电时序按照说明书中的流程进行,检查了寄存器的写入读取均无问题,SPI的通讯时序也无异常。
请问这是什么问题,可否说明一下VCAP4引脚电压异常说明芯片中的何种功能会出现异常,谢谢。
您好,
那您前面回复的时候提到,“vrefn引脚连接avss测得是-2.5V,vrefp测得是1.9V”,这个电压是是基于哪个地测试的?
如果仍然vcap4电压不对,请参考评估板检查电路设计。