This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3542: 配置寄存器后,采集输出波形不正常

Part Number: ADC3542


寄存器配置 地址 数据
1 x"0000" x"01"
2 x"0007" x"2B"
3 x"0013" x"01"
4 等待1ms
5 x"0013" x"00"
6 x"000A" x"FF"
7 x"000B" x"EF"
8 x"000C" x"FC"
9 x"0018" x"10"
10 x"0019" x"12"
11 x"001B" x"90"
12 x"001F" x"40"

具体寄存器配置如上所示,想到达到该截图的效果,不知配置是否正确,是否需要更改什么?