Part Number: ADS4229
使用ADS4229设计数据采集系统,一个系统上设计2块4229,每个ADC有2路数据输入,ADC1的采集数据正常,ADC2采集到的数据某一路会失真,如下图

2路信号中,红色的为方波,波形正常,橙色的是正弦波,明显失真,最大有7V电压,但是整个系统输入的电压只有0~2.5V。ADC输入的时钟、供电电压都是正常的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
可能原因:
输入信号范围:
共模电压(Vocm)问题:
时钟和供电:
信号完整性:
ADC配置: