This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI专家:
请教一个问题,DAC3162的datasheet上说输出端电压范围为(AVDD-0.5V至AVDD+0.5V),请问,该电压兼容是针对P或者N单个输出口而言还是说输出差分信号,如果是后者,那相当于输出差分电压最大幅值是1Vpp,如果是前者,那输出差分电压最大幅值可达2Vpp。根据datasheet后文,这里说的电压范围(AVDD-0.5V至AVDD+0.5V)应该指的是单端的限制。但是datasheet第5页中的注释说 Measured differentially across IOUTAP/N or IOUTBP/N with 25 Ω each to AVDD.按这里的意思又应该指的是差分的。
另外,datasheet第3页表格中名字为NC的Pin脚是从29-32,表中写成了25-32.
首先,DAC3162是电流输出DAC,如果你不接外部电路,那么讨论其输出电压是不合理的。
具体的电压范围可以参考 数据手册 19页 ANALOG CURRENT OUTPUTS 章节。
Dear Airwill:
能否解释下为什么输出信号不能超过AVDD?Datasheet上说范围是AVDD-0.5v--------------AVDD+0.5V,如果不能达到datasheet上这么说不是坑人吗。
Dear Martin:
我看了datasheet的,我也知道是电流输出需要接外接电路的。我就是看了19页的datasheet觉得输出电压可以到2Vpp,但是
第5页表格中有如下注释“Measured differentially across IOUTAP/N or IOUTBP/N with 25 Ω each to AVDD”,然后表格中的结果是Output compliance range AVDD– 0.5 AVDD+ 0.5。
5页中的测试条件是串25欧姆的电阻,而19页中相当于串了50欧姆的电阻对电源,那如果串100欧姆的呢?