Other Parts Discussed in Thread: DAC3162
Dear TI专家:
请教一个问题,DAC3162的datasheet上说输出端电压范围为(AVDD-0.5V至AVDD+0.5V),请问,该电压兼容是针对P或者N单个输出口而言还是说输出差分信号,如果是后者,那相当于输出差分电压最大幅值是1Vpp,如果是前者,那输出差分电压最大幅值可达2Vpp。根据datasheet后文,这里说的电压范围(AVDD-0.5V至AVDD+0.5V)应该指的是单端的限制。但是datasheet第5页中的注释说 Measured differentially across IOUTAP/N or IOUTBP/N with 25 Ω each to AVDD.按这里的意思又应该指的是差分的。
另外,datasheet第3页表格中名字为NC的Pin脚是从29-32,表中写成了25-32.