Other Parts Discussed in Thread: UNIFLASH, MSP-EXP432E401Y
Hello:
My BP-DAC11001EVM can not connect the GUI,and I Changed the Port COM6 or COM7 ,it still failed.



The MSP-EXP432E401Y EVM can be Autodetected by Uniflash,and I loaded the test program “


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello:
My BP-DAC11001EVM can not connect the GUI,and I Changed the Port COM6 or COM7 ,it still failed.



The MSP-EXP432E401Y EVM can be Autodetected by Uniflash,and I loaded the test program “blinky.bin”, the LED will flash. then I load the “acctrl.bin”, it not work.


您好,
请看这个软件的操作系统要求。
在安装过程中勾选 ( Always trust software from "Texas Instruments")
固件acctrl.bin更新完成后,
然后按照BP-DAC11001EVM User's Guide 的“2.2.2 Connecting the Hardware”,USB插入U7。
下面帖子讨论了类似问题,请参考
(+) BP-DAC11001EVM的硬件无法连接,显示Hardware not Connected - 数据转换器论坛 - 数据转换器 - E2E 设计支持

当我点击链接的图标时会显示等待数据中,但是最后会提示失败。
另外我有按照下图中的README提示替换了OCFSPI文件,也不行。

Temporary fix for the GUI Composer RunTime Version Mismatch:
Replace the OCFSPI.js file in (C:\Users\<user name>\guicomposer\runtime\gcruntime.v7\BP-DAC11001EVM\components\ti-core-databind\src\internal\reg\OCFInterfaces) by the file one in this directory.
您好,
请按照下面的步骤重新编程试一下
1、从机器上卸载EVM软件和runtime。
2、从GUI Composer Library下载EVM软件和runtime文件。
3、安装EVM软件和runtime(必须安装runtime引擎才能使EVM工作)
4、按照第2.1.2节中概述的步骤升级Launchpad上的固件(请按照概述的步骤进行操作)
5、 Cloud agent 安装。在此步骤之后,应该检测到launchpad 板。
6、加载固件映像并进行验证。
请确保acctrl.bin固件升级成功,然后USB插入U7测试连接,两个串口都试一下。
如果还不行,若是从TI store购买的评估板,请凭订单号联系Customer support center | TI.com