关于ADS1274数据采集这块已经花了一个多月的时间,通过一遍又一遍的看官方的说明文档已经解决了大部分的问题,目前仍然存在几个不懂的地方,希望TI工程师给解答一下;
问题1:在2011版说明文档中P26说到,Crystal clock oscillators are the recommended clock source.推荐使用晶体振荡器来给AD提供工作时钟,那么管脚晶振的选择有什么要求吗,有源的还是无源的,2个脚的还是4个脚的,又该怎样连接到CLK管脚呢,还需不需要加电容等,,,,目前是用MCU来提供CLK信号,感觉精度不够
问题2:在2011版说明文档中P35,有关POWER SUPPLIES的问题,ADS1274的三路电源上电顺序DVDD、IOVDD、AVDD,文中说的,这三路电源只有按照规定的顺序先后通电才会使ADS1274内部复位,我的电路图用的就是官方提供的参考电路图,是不是需要在这三路电源上分别接上开关呢?
麻烦哪位TI工程师出来解答一下,谢谢啦!