控制器板下载好bin文件,BP-DAC11001EVM上位机连接成功,但无法设置参数,寄存器也无法写入,会是什么问题呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
您是否能够从任何一个寄存器中读取?
是否可以尝试以下调试步骤:BP-DAC11001EVM: Unable to change output at TP6
GUI状态是否显示"Hardware Connected (硬件已连接)"?
2.如果是,请将LDAC模式更改为SYNC,并将Power Up/Down更改为 UP
3.跳线配置是否与下图所示相同-
4.如果DAC输出仍然没有变化,请检查下载的软件文件,并阅读readme.txt,网址为. ...\BP-DAC11001EVM_1.0.0_installer_win\install_image_BP-DAC11001EVM\BP-DAC11001EVM\app\patch\,然后按照说明进行操作。