This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

基于TI DLP4500的光谱仪设计若干问题咨询

Other Parts Discussed in Thread: DLPC350, DLP4500, TIDA-00155, DLPNIRSCANEVM, DLP4500NIR, DLPR350, AM3358

各位大神:

我司正在做基于DLP4500的光谱分析仪器,买了3套LightCrafter4500做参考设计,但是对于基于DMD的光谱仪到底怎么设计还不是很熟悉(由于英文水平实在不咋滴,看了3个星期的文档,说实话还是一头雾水)。我们现在是用外部的ARM cpu通过USB来配置DLPC350,用FPGA来传输哈达玛模板,主要疑惑有:

1.用作光谱分析仪器,DLPC350究竟该怎么配置?

2.怎么控制DMD进行扫描?即怎么根据哈达玛模板控制DMD上特定的列打开,特定的列关闭?

Jeremy 我发了邮件给您。

谢谢!

  • 1. DLPC350(NIR4500)参考设计请用:

    http://www.ti.com/tool/TIDA-00155

    http://www.ti.com/tool/dlpnirscanevm

    是使用的DLP4500NIR 的DMD.不是普通的lightcrafter4500.

    2. DLPC350 NIR的控制请参考UserGuide:

    http://www.ti.com/tool/dlpr350

    http://www.ti.com/lit/pdf/dlpu016

  • HI Jeremy

    我们知道DLP4500NIR是专门的近红外光谱仪,但我们一开始买的开发板买的是lightcrafter4500,而且买了

    好几套。后来了解到都是用DLPC350来控制的,所以控制方法是一样的,所以想先在lightcrafter4500开发板上做

    开发,熟悉DLPC350的控制方法。

    但是目前,我们对DLPC350怎么控制不是很了解,就是DLPC350怎么根据换哈达玛模板来控制微镜,文档翻来覆去看了几遍,

    也是模模糊糊的,能否具体讲解下:

    1、如何初始化DLPC350,使其能从我们外部的FPGA接收模板数据?

    2、怎么控制DLPC350,从接收到的模板数据,比如第一位接收到1,那么第一列的微镜全部打开,第二位接收到0,那么第二列的微镜全部关闭?

    期待您的解答,谢谢!

  • 1. DLPC350可以接收RGB(24BITS)数据;这个USER GUIDE有说明.配置为RGB,24BITS;

    2. TI Spectroscopy是使用AM3358来产生需要的PATTERN,(计算出哪些COLUMN选中).再传输给DLPC350.

    这个复杂的计算过程在:第11页. http://www.ti.com/lit/an/dlpa049/dlpa049.pdf

  • 自己看文档好几遍也是看不懂的。

    我就问下AM3358例程中的函数int dlpspectro_setup_50_50_seq_prgb(void),这个函数选中了哪些COLUMN?

    哪个命令是控制选中这些COLUMN的?

  •  通过我们沟通,如果你还有问题,请参考第10 页:http://www.ti.com/lit/an/dlpa049/dlpa049.pdf

    或参加我们workshop(8月2日或8月3日).