4500的外部触发输出和外部触发输入是在哪里,需要设置么?直接从3口连接到示波器没有信号。
Peripheral Control里的General Purpose Clock里面的两个输出 CLK_OUT1 和 CLK_OUT2 是哪两个输出口?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
4500的外部触发输出和外部触发输入是在哪里,需要设置么?直接从3口连接到示波器没有信号。
Peripheral Control里的General Purpose Clock里面的两个输出 CLK_OUT1 和 CLK_OUT2 是哪两个输出口?
谢谢!
参考64页J11输入触发.J14输出触发.
http://www.ti.com/lit/ug/dlpu011e/dlpu011e.pdf
如果你使用DLP-ALC-LIGHTCRAFTER-SDK-2.0,
DLP-ALC-LIGHTCRAFTER-SDK-2.0\TIDA-00254_LCr4500_MachineVision\src\config
在config_projector.txt
LCR4500_PARAMETERS_USE_DEFAULT = 1
##For below parameter
## 1 - External Positive Trigger
## 0 - Internal Trigger
LCR4500_PARAMETERS_TRIGGER_SOURCE = 1
请参考具体的timing模式:
第48页.
http://www.ti.com/lit/ug/dlpu011e/dlpu011e.pdf
我们这个速度是内部PATTERN.
只要保持同步即可.没有办法保持那末精密的.
Pattern period值480微秒对应的是2083HZ.