This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于3435搭配DLPA2005使用的工作电压问题

Other Parts Discussed in Thread: DLPA2005, DLPC3435

    一般是使用双节串联降压到5V给系统供电。

    我有一款产品,因为是使用micro接口给机器供电,电池选用了并联的电池。就是单节电池电压的意思。调试中,直接用直流稳压电源,加电给DLPA2005的VINL输入电压需要调到3.8V光机才能被点亮(稳压电源限流设置的5A),电容已经加得足够多了,开始两个22UF电容需要4.5V才能点亮。用的代理商给的flash程序,点亮时测量39mR的电阻电压为97mV。

    不能被点亮时表现为红灯闪烁一下,测量看是DLPA2005关闭了光机的那几组电源,是DLPA2005判断到电压低了不足以工作吗?但是外围又没有其他可调整的地方了。

目前还没有使用I2C来控制寄存器。看DLPA2005规格书中的7.3.7 Transient Current Limiting中有提到,上电时红灯会引起电流尖峰,不知道是否与这个有关系?ILIM[3:0]这个寄存器是在用TI的软件生成FLASH的程序中配置的吧?

生成FLASH的程序的这个配置软件可以提供一下吗?

   

  • 貌似负载电流太大了,电源纹波大。再研究一下。

  • 请在开机时测试一下DLPA2005的VIN电压波形,看是否有过冲或较大纹波。还可以测试一下5V Vin是否工作正常。

    Transient Current Limiting寄存器是用来限制LED灯的尖峰电流,一般不会影响开机。参数设置用默认的就好。

    建议你再测试一下光机厂提供的flash程序。如果需要修改DLPC3435的初始化配置,请联系光机厂家帮忙修改。