This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教 3435+PAD3000 3000的10V 18V -14V没有输出 3435 HOST_IRQ一直高

Other Parts Discussed in Thread: DLPC3435

pad3000的上电时序,在Reset 信号出现后,时序都是正常的。 就是PAD3000的 10V 18V -14V没有输出。 3435的SPI  FLash 数据和时钟都有观察到波形,感觉程

序应该有跑, DMD排线没有做阻抗 也没有走差分,不知道是不是这里的原因?  PAD3000的这几个电压,是不是需要3435程序启动后,通过SPI1和PAD3000通讯来

设置?