1.使用直接下载的编译好的3D_Scan_Application_V2,在利用菜单“2”生成固件是产生的投影图0和1正确无误
2.然而使用SDK2.0中的源代码自行编译的Application,在生成投影时投影图1错误,而0正确,如附件所示
请问什么原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.使用直接下载的编译好的3D_Scan_Application_V2,在利用菜单“2”生成固件是产生的投影图0和1正确无误
2.然而使用SDK2.0中的源代码自行编译的Application,在生成投影时投影图1错误,而0正确,如附件所示
请问什么原因?
附件内为生成的固件,请查收,谢谢
对了,编译环境为ubuntu16.04,opencv2.4.9.1, FC驱动为官网最新
1.请提供config 目录下文件(包含DLP_LightCrafter_4500_3D_Scan_Application_Config.txt)
2. 请也提供:
dlp_sdk_lcr4500_dlpc350_prepared.bin.flash_image_0.bmp
dlp_sdk_lcr4500_dlpc350_prepared.bin.flash_image_1.bmp
dlp_sdk_lcr4500_dlpc350_prepared.bin.flash_image_2.bmp
.....
等图片文件.
谢谢!需要configure目录下所有的文档:
config_projector.txt
calibration_camera.txt
geometry.txt
config_camera.txt
algorithm_horizontal.txt
algorithm_vertical.txt
calibration_projector.txt
等.
我们在基于linux系统的AM5728测试同样配置没有问题的。请参考:
http://www.ti.com/tool/tidep0076
http://www.ti.com/tool/TMDSEVM572X
和编译过程user guide:
http://www.ti.com/lit/ug/tiduc48a/tiduc48a.pdf