分别用TI lightcrafter 4500与lightCrafter3000触发信号相机。用示波器采集TI lightcrafter 4500与lightCrafter3000触发信,示波器显示脉冲高度0.4v,原因小于3.3v,无法触发相机。请问是哪里的问题,以前有同事用过,输出脉冲是2.8v,接近3.3v。请问如何处理才能得到接近3.3v的投影仪触发脉冲。
非常感谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
分别用TI lightcrafter 4500与lightCrafter3000触发信号相机。用示波器采集TI lightcrafter 4500与lightCrafter3000触发信,示波器显示脉冲高度0.4v,原因小于3.3v,无法触发相机。请问是哪里的问题,以前有同事用过,输出脉冲是2.8v,接近3.3v。请问如何处理才能得到接近3.3v的投影仪触发脉冲。
非常感谢
您好,感谢您的帮助。
根据您的建议,我测试了J7pin1的电压,电压为0.4v。另外,我用示波器测U23的引脚,测的和J7的pin3引脚波形类似,都是为脉冲,但是脉冲电平仍然为0.4v。
具体结果如下:
图1为J7Pin3引脚输出波形,U23的某一引脚的波形也类似。
图1 J7 Pin3引脚波形
图2为J7的Pin1和Pin3引脚。(图2中,探针连接的引脚输出波形电平也为0.4v左右。)
图2 实验波形对应引脚图
另外,U23有的引脚不是脉冲,信号也是0.4v左右。
总之,没有得到3.3v的电压或者脉冲信号。如何得到3.3v的脉冲,可以再给些建议吗?
另外,还想请教一个问题。现在我采用的是J7引脚触发Pointgrey相机。但是我参考的Ti lightcrafter J7引脚与imagesource相机的连接方式。Ti官方J7与imagesource相机触发连接的文献是J7的Pin1与Pin3引脚与image source相机的触发端相连。对于pointgrey相机,我采用同样方式将pointgrey相机端触发端的信号与地分别与J7的Pin3 与Pin1引脚连接。但是现在想想,是不是应该与J7的Pin3与Pin4连接才对?是不是因为我引脚接错了,烧坏了lightcrafter导致现在输出电平0.4v左右?相机触发端的地需要与Pin1引脚连接还是与Pin4引脚连接?
谢谢!
您好!
从您的描述来看,EVM的供电可能出现了问题。尤其是3.3V电源,请根据原理图仔细检查板卡供电是否正常。造成这个的原因很有可能是因为将Camera的ground连接到了J7的1脚上。
pin1电源的用处在于,通常camera的工作电压是不一定的,为了兼容不同的camera,使用pin1作为camera为system board的供电引脚(仅限于)U20和U23.
如果使用Point Grey的camera,且是camera触发evm则使用pin2和pin4,反之则应该是pin3和pin4,camera端请参考它的datasheet。
这是TI的reference Design的设计,请参考:



Page25