产品:DLP® LightCrafter™ Evaluation Module (EVM)
操作系统: win7,64位操作系统
安装的GUI版本:DLPLCR_GUI_SRC_v4.0.1_WIN_2013_07_19
问题描述:
1、使用miniUSB数据线,将PC与DLP Lightercrafter连接。
2、参照“dlpu006e.pdf”中第14页—>“2.2.2 Installing the RNDIS Driver on Windows 7”。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
感谢您关注TI的DLP产品。
DLP3000已经EOL了,TI并不推荐任何基于DLP3000的项目开发或者评估。
您可以选择DLP3010-LC EVM或者DLP2010-LC EVM,请参考:



谢谢。