This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Lightcrafter 参照“dlpu006e.pdf”中第14页,无法连接



产品:DLP® LightCrafter™ Evaluation Module (EVM)

操作系统: win7,64位操作系统

安装的GUI版本:DLPLCR_GUI_SRC_v4.0.1_WIN_2013_07_19

问题描述:

1、使用miniUSB数据线,将PC与DLP Lightercrafter连接。

2、参照“dlpu006e.pdf”中第14页—>“2.2.2 Installing the RNDIS Driver on Windows 7”。