This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01226 EVM电路中U48位置的CY7C65215-32LTXI问题



你好

       我新做的板把EVM电路中USB转I2C(U48位置CY7C65215-32LTXI)的这部分电路保留了,但是调试时发现无法使用,这个芯片是要下载配置文件吗?哪里可以下载?或者是否可以发我的邮箱luoxiucai@hotmail.com

  • 您好!
    感谢您使用TI的DLP产品。
    非常遗憾碰到这个问题,但是这款芯片并不是TI的产品,推荐您去找到Cypress Semiconductor Corporation的技术支持询问。
    除此之外,是否有其他可以帮助到你的?
  • 你好
    我找Cypress Semiconductor Corporation的技术支持也不一定能解决,应该是TI这边配置一些特定的PID/VID和设备码之内的
  • 你好

           这个Licesene是TI的,这边是否可以提供呢?

    DLP LightCrafter Display Manifest Table

    See the Legend above for a description of these columns.

    Software Name Version License Type Delivered As Modified by TI
    DLP LightCrafter™ Display See release-notes.rtf file TI Commercial License Binary Yes Location User selectable installation directory. Typically C:\Program Files (x86)\DLP LightCrafter Display xx.xx where xx.x.x is the current version number.
    Obtained from TI
    Boost 1.32 BSL-1.0 Binary Yes Location Included in DisplayCrafter Software binary.
    Obtained from http://www.boost.org
    Zlib 1.2.3 Zlib License Binary No Location File zlibwapi.dll in user selectable installation directory. Typically C:\Program Files (x86)\DLP Composer xx.xx where xx.x.x is the current version number.
    Obtained from http://www.zlib.net/
    MFC Grid Control 2.25 Code Project Open License 1.02 Binary Yes Location Included in DisplayCrafter Software binary.
    Obtained from http://www.codeproject.com/KB/miscctrl/gridctrl.aspx
    The MFC Answer Book Addison Wesley-Longman & Eugene Kain Binary Yes Location Included in DisplayCrafter Software binary.
    Obtained from The MFC Answer Book, by Eugene Kain
    Cypress USB Serial driver 1.2.3.31.0.0.74 TI Commercial License Binary No Location User selectable installation directory. Typically C:\Program Files (x86)\ DisplayCrafter xx.xx\Drivers\Cypress where xx.x.x is the current version number.
    Obtained from http://www.cypress.com/?rID=83110
  • 你好

          这个Licesene是TI的,这边是否可以提供呢?

    DLP LightCrafter Display Manifest Table

    See the Legend above for a description of these columns.

    Software Name                      Version License     Type                                    Delivered As     Modified by TI  

    Cypress USB Serial driver    1.2.3.31.0.0.74         TI Commercial License      Binary               No                        

  • 您好!

    很抱歉目前TI并没有在ti.com上发布该文件。

    但是我在英文E2E上找到了一个替代的解决方案,您看是否可行?请参考