你好
我新做的板把EVM电路中USB转I2C(U48位置CY7C65215-32LTXI)的这部分电路保留了,但是调试时发现无法使用,这个芯片是要下载配置文件吗?哪里可以下载?或者是否可以发我的邮箱luoxiucai@hotmail.com
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好
我新做的板把EVM电路中USB转I2C(U48位置CY7C65215-32LTXI)的这部分电路保留了,但是调试时发现无法使用,这个芯片是要下载配置文件吗?哪里可以下载?或者是否可以发我的邮箱luoxiucai@hotmail.com
你好
这个Licesene是TI的,这边是否可以提供呢?
DLP LightCrafter Display Manifest Table
See the Legend above for a description of these columns.
| Software Name | Version | License Type | Delivered As | Modified by TI | ||
| DLP LightCrafter™ Display | See release-notes.rtf file | TI Commercial License | Binary | Yes | Location | User selectable installation directory. Typically C:\Program Files (x86)\DLP LightCrafter Display xx.xx where xx.x.x is the current version number. |
| Obtained from | TI | |||||
| Boost | 1.32 | BSL-1.0 | Binary | Yes | Location | Included in DisplayCrafter Software binary. |
| Obtained from | http://www.boost.org | |||||
| Zlib | 1.2.3 | Zlib License | Binary | No | Location | File zlibwapi.dll in user selectable installation directory. Typically C:\Program Files (x86)\DLP Composer xx.xx where xx.x.x is the current version number. |
| Obtained from | http://www.zlib.net/ | |||||
| MFC Grid Control | 2.25 | Code Project Open License 1.02 | Binary | Yes | Location | Included in DisplayCrafter Software binary. |
| Obtained from | http://www.codeproject.com/KB/miscctrl/gridctrl.aspx | |||||
| The MFC Answer Book | Addison Wesley-Longman & Eugene Kain | Binary | Yes | Location | Included in DisplayCrafter Software binary. | |
| Obtained from | The MFC Answer Book, by Eugene Kain | |||||
| Cypress USB Serial driver | 1.2.3.31.0.0.74 | TI Commercial License | Binary | No | Location | User selectable installation directory. Typically C:\Program Files (x86)\ DisplayCrafter xx.xx\Drivers\Cypress where xx.x.x is the current version number. |
| Obtained from | http://www.cypress.com/?rID=83110 |
你好
这个Licesene是TI的,这边是否可以提供呢?
DLP LightCrafter Display Manifest Table
See the Legend above for a description of these columns.
Software Name Version License Type Delivered As Modified by TI
Cypress USB Serial driver 1.2.3.31.0.0.74 TI Commercial License Binary No
您好!
很抱歉目前TI并没有在ti.com上发布该文件。
但是我在英文E2E上找到了一个替代的解决方案,您看是否可行?请参考