你好!
看PAD2005的规格书,在VLED电压2.8V-4.8V的范围内,可以提供最大2.5A的电流。在输入电压满足4.5V-5.5V,效率可以达到87%以上。现在我们的产品,在低功率时(ILED≤2.1A)效率基本可以达到85%左右,但是如果LED电流在加大,效率就会降低到60%-65%左右。请问这是为什么呢?是软件设置问题还是硬件设计存在缺陷?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!
看PAD2005的规格书,在VLED电压2.8V-4.8V的范围内,可以提供最大2.5A的电流。在输入电压满足4.5V-5.5V,效率可以达到87%以上。现在我们的产品,在低功率时(ILED≤2.1A)效率基本可以达到85%左右,但是如果LED电流在加大,效率就会降低到60%-65%左右。请问这是为什么呢?是软件设置问题还是硬件设计存在缺陷?