This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、如何通过USB或者I2C对DLPC910的寄存器进行配置,是否有相应的软件提供,此外,
2、TIDA-00570参考设计中,电路板上电后,ECP_FINISHED信号并未拉高,DLPR910PROM中的程序并未加载成功,可能的原因有哪些,手册上写道,只要上电就会自动P加载PROM程序。给DLPC910写入亮灯程序,芯片正常工作。目前只有TIDA-00570主板,没有DMD板,这是否影响PROM程序的自动加载。
3、DLPR910是经过编程的,如果给它下载其他的程序,芯片原来配置程序是否还可以使用。
望解答!
您好!
感谢使用TI的DLP产品。
1.目前DLPC910并没有相应的控制软件在,但是ti的第三方合作伙伴可以提供相应的软件,您也可以考虑从design house处获取
http://www.ti.com/product/DLPC910/toolssoftware
2.请问目前您的参考设计是自己设计的吗?如果是采购的第三方的建议您向其索取setup的user guide。没有DMD板应该并不会影响FPGA载入配置文件,但是我需要double confirm。
3.DLPR910是不能编程的,TI并不提供相应的固件,并且也没有办法从PROM中读出固件,因为prom具有读保护。
Best regards
您好!
1.建议您与TI的参考设计做对比,检查有哪些修改。另外检查上电后板子的电源轨是否正常,尤其检查DLPC910和DLPR910的电源轨是否正常已经在规格要求范围内。
2.这些操作需要控制输入DLPC910的信号来实现的,N/S Flip通过配置ROWMD实现,模式控制需要配合RST2BKLZ、BLKMD、BLKAD已经输入数据等信号来实现,具体请参考DLPC910数据手册7.4章,有详细说明。
http://www.ti.com/lit/ds/symlink/dlpc910.pdf
Best regards