1、如何通过USB或者I2C对DLPC910的寄存器进行配置,是否有相应的软件提供,此外,
2、TIDA-00570参考设计中,电路板上电后,ECP_FINISHED信号并未拉高,DLPR910PROM中的程序并未加载成功,可能的原因有哪些,手册上写道,只要上电就会自动P加载PROM程序。给DLPC910写入亮灯程序,芯片正常工作。目前只有TIDA-00570主板,没有DMD板,这是否影响PROM程序的自动加载。
3、DLPR910是经过编程的,如果给它下载其他的程序,芯片原来配置程序是否还可以使用。
望解答!