This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP®︎ NIRscan™︎ Nano 源代码编译错误 identifier is undifined



我们购买了DLP NIRScan Nano EVM模块,从TI官网下载了源代码Mobile Spectroscopy TIVA EVM,编译出现了两个错误。该错误由其他工程师于2019年在TI官方英文社区反馈过,没有解决。求助TI专业工程师帮助解决。

产品链接如下:www.ti.com/.../DLPNIRNANOEVM

错误如下

1.Description Resource Path Location Type
#20 identifier "calibCoeffs" is undefined cmdDict.c /Mobile Spectroscopy TIVA EVM/App line 75 C/C++ Problem

2.Description Resource Path Location Type

#20 identifier "scanConfig" is undefined cmdDict.c /Mobile Spectroscopy TIVA EVM/App line 64 C/C++ Problem

可以提供的信息如下:

1. 操作系统版本:windows10 1903 64bit

2.CCS  version:

安装信息如下:6.0.1.00040 

3.其他软件安装信息:

4. project building setting

因为我们没在TI官网找到 TI ARM compiler 5.2.4,因此安装了5.2.9版本。

a.

b. RTSC setting

5.我们严格按照DLP® NIRscan™ Nano EVM User's Guide page 61~66进行安装和编译。

6.在按照user guide page64 C.1.3进行编译的时候,发现上图中dlpspeclib出现黄色叹号。如下图所示,但各种操作均按官方user guide进行。

包含的警告信息如下;

7.补充信息

我们在TI论坛其他位置也发现了其他用户相同的反馈,但未给出解决办法

e2e.ti.com/.../849241