DLP4710 LC套件,在使用的过程中,不需要内置的光源,如何去掉这三个光源? 目前去掉LED,就无法正确投影图像。 是否可以通过在硬件上对PMIC管理芯片的反馈引脚做一定处理,如R595这个电阻的输入信号给特定信号,以避免外接光源? 还是在软件上,可以更新固件,不让PMIC检测LED开路的问题?
在英文论坛搜到相关回答,但是找不到固件的资源和下载路径:
For the DLPC3479 chipset we allow multiple options (single option at a time).
you can pick any one below option depends on your requirement and design.
We could provide you the firmware based on your need :
1. No LED connected to DLPA3005
2. Any one LED connected to DLPA3005
3. Any two LEDs connected to DLPA3005
这是否是软件的一种解决办法?
谢谢!