This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3478: 配合dlpa2005使用但是resetz信号每200ms出现一个低电平

Part Number: DLPC3478
Other Parts Discussed in Thread: DLPA2005

DLPA2005+DLPC3478初始化出现问题不了,Host-irq一直为高。后来发现是resetz信号周期性的一个低电平,约200ms左右。请问是什么原因造成的?

  • Host_IRQ信号没有拉低,说明系统初始化有问题。常见的解决思路是,先检查DLPC芯片和DMD的供电是否正常,然后确认DLPC外挂的Flash已经烧录了对应的固件。在上电过程中可以测试一下DLPC有没有读flash,和DMD的LS信号是否正常。如果DLPA2005的ResetZ信号异常,可以检查一下2005外围电路是否正常。