This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3010EVM-LC: 显示一系列1-bit图案 并与相机同步

Part Number: DLP3010EVM-LC
Other Parts Discussed in Thread: DLP3010, DLP3010LC, DLP4500

您好,我正在使用DLP3010EVM-LC,我想请问怎么控制dmd显示一系列二维1-bit(黑白)图像,大概2000张。我希望每张图像显示的时候会有一个output trigger,以便相机同步捕捉这个图像。

我一开始用HDMI线将DLP和电脑连在一起,可是这样就不能控制显示图案和触发的同步。可是Light control模式下的internal pattern只能显示一维图案,但我想显示二维图案。请问DLP3010有没有像DLP Lightcrafter 4500那样的pattern sequence模式呀?

还有如下问题:

1. 请问我需要将图案烧录到flash里吗?如果需要的话应该怎么做呢

2. 我用跳线连接了J11的Pin2和Pin3以达到3.3V的输出电压,但是用示波器显示J4的trigger out波形时,仍然只显示156mV