This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC410: 同步信号

Part Number: DLPC410


 工程师您好!上面说的是GPIOA0产生的同步信号,编程文件说的是控制GPIOA1,是错了吗?还有以下一些疑问希望解答。如有相关程序范例是否能提供?非常感谢

1、DLP4100进行编程控制可以使用什么软件啊?

2、需要通过同步信号脉冲触发采集卡进行采集数据,请问是否有相关范例提供,非常感谢您的解答。

  • GPIOA1 是指FPGA上面的管脚。

    DLP4100进行编程需要什么软件取决与你们系统需要PC还是其他处理芯片对DLP4100控制然后选择。 FPGA/DLPC410的软件都不需要编程。

    采集数据是指什么?我们目前有的是API代码以及编程指南。

  • 谢谢您的回答,主要是通过PC对DLP4100控制,采集数据是探测器收集光强信息再通过NI数据采集卡进行采集,是否能通过DMD镜面翻转信号作为外部触发采集卡进行采集数据这样的范例?