This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3478: 关于用DLPC3478的GUI “Run Once”一次投影后,DLPA3005的VRST\VBIAS\VOFS电压将不再输出,不知道为什么?输出前实测Vrst=-14.33V,Vbias=17.7V,Vofs=9.89V。

Part Number: DLPC3478
Other Parts Discussed in Thread: DLPA3005, , DLPA3000

尊敬的TI技术,你们好:

现在我做的产品的情况如下:

1、产品的方案是DLPC3478+DLPA3005;

2、产品采用的img是dlpc347x_7.0.0.img,默认是“Splash Screen”,仅仅打开了蓝灯;

3、产品首先通过处理器的I2C配置DLPC3478工作模式是“Internal Pattern Streaming”模式,然后用GUI烧入如下文件,配置蓝灯工作。

目前出现问题和现象如下:

a、在“Splash Screen”情况下,能够正常常亮投出图片;

b、配置“Internal Pattern Streaming”模式后,用DLPC3478的GUI “Run Once”一次投影成功后,DLPA3005的VRST\VBIAS\VOFS电压将不再输出。 “Run Once”前实测Vrst=-14.33V,Vbias=17.7V,Vofs=9.89V;“Run Once”后Vrst、Vbias、Vofs实测都为0。

c、尽管Vrst、Vbias、Vofs输出为0后,I2C依然还可以与DLPC3478通信,可以read、write数据。但是尽管配置“Splash Screen”模式后,仍是无法点亮灯珠。

请TI的大牛帮忙分析下,多谢!