Other Parts Discussed in Thread: DLP5531-Q1
There is no problem with the bin file flash and verification process, but the reset process keeps reporting errors at the end. I don't know how to solve it. And the circuit board lit up with red lights.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There is no problem with the bin file flash and verification process, but the reset process keeps reporting errors at the end. I don't know how to solve it. And the circuit board lit up with red lights.
你的板子是自己做的吗?请检查DLPC, DMD和TPS99000的标号是否配套,TI有两个版本,后缀有S和无S的两种芯片。你们的bin文件是官网直接下载的吗?
是从官网购买的套件,并按指导组装,已经正常使用约2年了。bin文件是官网下载的,更改了几张图片,昨天只是重新加载了bin文件,之前已经进行过多次同样的操作了,但是在加载后,refresh flash成功,但是无法reset,也就无法进入display模式,同时注意到板上亮起一个红灯,我不知道这意味着什么,谢谢您,期望得到您的帮助
用默认的EVM固件试一下,看看能否正常工作。如果能工作,再查找一下你自己做的固件是否有问题。建议先少改几个地方,一步一步试。
您好,我没有自己添加固件,就是从官网配套购买的DLP5531-Q1一整套,只是重新加载了一个bin文件,在加载之后就无法完成reset,谢谢您的的建议