This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3439: HDMI输入Video模式下Parallel Interface问题

Part Number: DLPC3439


Ti工程师,您好:

目前是硬件方案3439+IT6801,IT6801输出RGB888信号(24bit)至双3439。

目前测试发现如下问题:

如果给光机输入的HDMI信号是RGB565(16bit),会发现图像像素的亮度有异常,比如像素该亮的地方暗了,

猜想可能是像素的字段对应有问题。

所以请Ti工程师确认以下问题:

1.如果给的HDMI源输出是RGB565,会在HDMI中表示它是RGB吗,光机会如何处理这16bit?

2.是不是IT6801收到信号后会把RGB565(16bit)t转换为RGB888(24bit)然后给到双3439?

3.看3439规格书介绍,3439确认是支持输入RGB565信号吗?

如果确认支持,意思是不是3439的硬件IO线只需要连接PDATA 0-PDATA 15,

然后在软件更改Write External Video Source Format Select,

然后3439内部会自动转换成RGB888,dmd就能正确显示?

4.如果我的第三点理解没有错,假设想正常的使用RGB565(16bit),

目前我的硬件方案是是hdmi那边不支持,需要更改hdmi芯片及Io pin连线才能使用?