Part Number: DLPC7540
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
切换Test Pattern和HDMI信号的dbmsg, 供参考!
Blank screen is set to TPG
dispfmt_CalculateDisplayArea: X, Y, Width, Height = 0, 0, 3840, 2160
dispfmt: minPan, pan, maxPan:0, 0, 0
data = { 3840, 0, 3840 }
dispfmt: minScan, scan, maxScan:0, 0, 0
data = { 2160, 0, 2160 }
dispfmt_CalculateCroppedArea: X, Y, Width, Height = 0, 0, 3840, 2160
dispfmt:apply_disp: activeSource = 3, dispSrc = 0
datapath: Transition to IDLING on Vx1(ITE0)
Command 0x11 execution took 215698 us (greater than allowed 50 ms)
mbSend: mbx: 2b610 msg: 0005 tID: 2b348
mbRecv: mbx: 2b610 msg: 0005 us (greatesource: SPLASH address: 0x1053045c
source: DisplaySplash size = 3840 x 2160
Blank screen is set to splash
dispfmt_CalculateDisplayArea: X, Y, Width, Height = 0, 0, 3840, 2160
dispfmt: minPan, pan, maxPan:0, 0, 0
data = { 3840, 0, 3840 }
dispfmt: minScan, scan, maxScan:0, 0, 0
data = { 2160, 0, 2160 }
dispfmt_CalculateCroppedArea: X, Y, Width, Height = 0, 0, 3840, 2160
dispfmt:apply_disp: activeSource = 2, dispSrc = 2
------------------- SCANNING CONNECTOR : Vx1(ITE0) ----------------
Warning: No AFE1000/HW communcation found while attempting to place stand-by (However connector table seem to have a VGA entry)
digcontrol: Decoder 5 powerStandby complete
digcontrol: ConfigureForSearch complete
datapath: Transition to SCANNING on Vx1(ITE0)
Event: Source Change Detected on channel
mbSend: mbx: 2b610 msg: 0004 tID: 28798
mbRecv: mbx: 2b610 msg: 0004 data:0000
Event: DSM Locked on channel
mbSend: mbx: 2b610 msg: 0003 tID: 28798
mbRecv: mbx: 2b610 msg: 0003 data:0000
digcontrol: FillSourceConfig - srcConfig:
TotalArea.PixelsPerLine - 4400,
TotalArea.LinesPerFrame - 2250,
ActiveArea.FirstPixel - 384,
ActiveArea.FirstLine - 82,
ActiveArea.PixelsPerLine - 3840,
ActiveArea.LinesPerFrame - 2160,
PixelClockFreqInkHz - 297000,
inputFrameRate - 60,
srcColorType - YUV420.
srcConfig->IsInterlaced - FALSE,
digcontrol: FillSourceConfig complete
Is3D = FALSE
dispfmt: DEI Disabled, Field Scaling Disabled
dispfmt: Input frame rate is 60Hz
dispfmt: input resolution: 3840 x 2160
dispfmt_CalculateDisplayArea: X, Y, Width, Height = 0, 0, 3840, 2160
dispfmt: minPan, pan, maxPan:0, 0, 0
data = { 3840, 0, 3840 }
dispfmt: minScan, scan, maxScan:0, 0, 0
data = { 2160, 0, 2160 }
dispfmt_CalculateCroppedArea: X, Y, Width, Height = 0, 0, 3840, 2160
dispfmt:apply_disp: activeSource = 0, dispSrc = 0
******* Try to set Color Profile 0 *******
pictcont: Active Display is 0
pictcont: Set White Peaking: 0
pictcont: Set gamma 0
pictcont: Sharpness 0
pictcont: cscIndex 0
pictcont: tableIndex 4
datapath: Transition to MONITORING on Vx1(ITE0)