Part Number: DLP3010
Other Parts Discussed in Thread: DLPA3000
你好。
我司在使用一片DLP3010的时候,出现工作一段时间后被击穿的现象,取下来进行检查发现VRST管脚对地电阻仅有5欧姆,外观无任何异常。我们想确定问题的原因,ESD/热/电击穿,结果在OM显微镜下出现了下面的图像,猜测可能是问题点。

请问针对可能的原因或者下一步的排查方向,是否有什么建议呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你测试给DMD的电压是否超标(波形),这是典型的电路问题。
非常感谢你的回复。
我这边测试VRST电压范围基本还是符合范围的,-13.9V的锯齿波,范围+-0.4V。
只是走线长度超过4000mil是否偏长?我怀疑是否因自感问题导致偶尔电压超标。
是否可以等比例增大三个电压的电容值呢?比如0.47uF/0.22uF/0.22uF同时再增加10倍的电容以做储能和错频带滤波?是否三个电压可以加上磁珠进行高频滤波?
另外,看了您推荐的这个pdf,同样是DLPA3000驱动DLP3010的架构,其layout指导确实对我的设计很有帮助。
任何超出规格书范围都会导致DMD 损坏。需要监测电压最恶劣的情况不能超标。