现在使用dlpc2607,投影出来的图象偏蓝,
1: 硬件接口采用RGB565方式,
PDATA[0~4] 端口接B[0~4]数据口
PDATA[5~10] 端口接G[0~5]数据口
PDATA[11~15]端口接R[0~4]数据口
2: IIC通信设定
addr 0x0b=0; //输入源选择
addr 0x0c=12; //800X480分辩率
addr 0x0d=0; //RGB565格式
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
现在使用dlpc2607,投影出来的图象偏蓝,
1: 硬件接口采用RGB565方式,
PDATA[0~4] 端口接B[0~4]数据口
PDATA[5~10] 端口接G[0~5]数据口
PDATA[11~15]端口接R[0~4]数据口
2: IIC通信设定
addr 0x0b=0; //输入源选择
addr 0x0c=12; //800X480分辩率
addr 0x0d=0; //RGB565格式
硬件的接法是对的, 检查一下光机的LED灯(红、绿、蓝)是否都有点亮。另外还可以测量一下RGB565的信号是否都有输入给DLPC2607。
通过IIC 通信将地址0xa6传不同值测到红绿那蓝正常,
投影模块是采购的,模块有自带测试图片,色彩都正常,
就是通过数据接口,传视频数据显示就偏蓝,将硬件接口接成RGB666及IIC也重新设置,显示也是偏蓝,
视频接口接上LCD显示屏颜色正常,
不知问题出在哪。
Display Curtain Control (I C: 0xA6, Flash: 0x000000A6)
Bits Description Reset Type
3:0 Display Curtain Enable (all undefined values are reserved) x0 wr
x0 = Curtain disabled
x1 = Curtain enabled
7:4 Display Curtain Color Select (all undefined values are reserved) x0 wr
X0 = Black x3 = Yellow (Red + Green)
x1 = Red x5 = Magenta (Red + Blue)
x2 = Green x6 = Cyan (Green + Blue)
x4 = Blue x7 = White