我把图片添加到firmware然后upload之后可以显示FLASH中的图像了。如果我第二次想重新显示flash里面的图片,但是又不想重烧固件,请问有没有什么办法可以重复多次显示里面的图片?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果是Lightcrafter4500是这么操作的.
如果是4500 3D printer TI参考设计,得修改GUI 软件代码:
buildimages.cpp中BuildImages().
可以增加一个变量:update_images;
void BuildImages(int led_current, float exposure_time, unsigned int image_count,
std::vector<std::string> print_images, dlp::LCr4500 *projector,
volatile bool *lcr4500_programming, bool update_images)
{
----
----
if(update_images)
{
// Call the prepare pattern sequence method from the LightCrafter 4500.
// This creates images and firmware from the sequence of patterns created
// earlier and sends it to the LightCrafter EVM
ret = projector->PreparePatternSequence(sequence);
// Print any errors from the pattern sequence preparation to the console
if(ret.hasErrors())
std::cout << (ret.GetErrors()).at(0) << std::endl;
dlp::Time::Sleep::Seconds(1);
}
----
----
}