This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教关于DLP4500的一个问题



我把图片添加到firmware然后upload之后可以显示FLASH中的图像了。如果我第二次想重新显示flash里面的图片,但是又不想重烧固件,请问有没有什么办法可以重复多次显示里面的图片?

谢谢!

  • 请参考http://www.ti.com/lit/pdf/dlpu011

    第51页关于*.ini的配置即可.(save solution).

  • 您好,我的意思是不重新传图片给4500,而是有什么指令或者外部触发,让它第二遍能重新显示flash里面的图片。谢谢!

  • 如果是Lightcrafter4500是这么操作的.

    如果是4500 3D printer TI参考设计,得修改GUI 软件代码:

    buildimages.cpp中BuildImages().

    可以增加一个变量:update_images; 

    void BuildImages(int led_current, float exposure_time, unsigned int image_count,

                     std::vector<std::string> print_images, dlp::LCr4500 *projector,

                     volatile bool *lcr4500_programming, bool update_images)

    {

    ----

    ----

       

    if(update_images)

    {

        // Call the prepare pattern sequence method from the LightCrafter 4500.

        // This creates images and firmware from the sequence of patterns created

        // earlier and sends it to the LightCrafter EVM

        ret = projector->PreparePatternSequence(sequence);

     

        // Print any errors from the pattern sequence preparation to the console

        if(ret.hasErrors())

            std::cout << (ret.GetErrors()).at(0) << std::endl;

     

        dlp::Time::Sleep::Seconds(1);

    }

    ----

    ----

    }

  • 好的,谢谢。我试试!