Part Number: DLPLCR65EVM
Hi all,
When I used product "DLPC900-DLP6500", I find that it will project black pattern ("all 0") with an angle of -12° between two patterns in a sequence although I have set the dark time to be 0. But I want it can project white pattern ("all 1") with an angle of +12° between two patterns to remove the distraction. I guess the reason for this problem is that dmd is project all black pattern by default when it is on standby or be stopped. So I was wondering if and how I can change the standby pattern to be another, for example all white ("all 1"), to solve this problem. Thanks for your kindly help.
Sincerely,
SQ