TI-API: V2 Backlog API Push Setup - ANYO PIONEER MOTOR INFORMATION #184598 - Order PUSH NOT RECEIVED in TEST ENVIRONMENT

Part Number: TI-API


Hell team,

Customer stated that they hadn't received any order push from TI test environment after 4/9 order creation. Please kindly check  and provide Order PUSH raw data. Thank you.

  • Hi Hazel,

    客户URL返回如下502报错,需要麻烦客户检查一下他们那边的设置。可以参考FAQ 贴 e2echina.ti.com/.../faq-push-api

    {
    "OrderNumber" : "1021708151",
    "CustomerPurchaseOrderNumber" : "TESTFOXSS-01",
    "CustomerAPIResponseStatusCode" : "502",
    "CustomerAPIResponseDateTime" : "2024-04-09 23:12:44",
    "CustomerAPIResponseStatus" : "FAIL",
    "CustomerAPIResponseMessage" : "java.io.IOException: Server returned HTTP response code: 502 for URL: ">101.230.151.155:10443/.../order_push",
    "CustomerAPIResponseContent" : "[Function: Call Customer API, Scripting]: Error executing custom script: Server returned HTTP response code: 502 for URL: 101.230.151.155:10443/.../order_push (in groovy2 script); Caused by: Server returned HTTP response code: 502 for URL: 101.230.151.155:10443/.../order_push (in groovy2 script); Caused by: Server returned HTTP response code: 502 for URL: ">101.230.151.155:10443/.../order_push"
    }

  • Hello Lecheng, Seeburger is fixing this issue with Anyo and will get back to us once it is sorted out. Thanks.