This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1043A-Q1: 唤醒问题

Part Number: TCAN1043A-Q1


我们使用TCAN1043有个这样的问题

上电启动时。VSP会供电12V,其它电源VDDIO_AON_3V3以及VDD_CAN_5V均没有供电,CAN总线上没有接设备,其它信号接的SOC或者悬空。

我们测试发现上电4分钟左右,INH才会拉低。

我看手册应该350ms就会拉低的,这是因为什么啊?

因为INH不拉低,我整个ECU的静态功耗在56uA,INH拉低后ECU功耗在26uA左右