The usb 2.0 hub desi
gn is follow TUSB4041PAPEVM Schematic. And use the external eeprom for PID/VID setting. The eeprom bin file is showed as picture.
In our application, the Host is the Mac mini (mac OS system). The hub is used to communicate with our product, and the product will power cycle which means the device will disappear and reconnect.
There exist a strange phenomenon: if the hub first power on ; or mac mini restart ; the hub will drop (the mac mini can't read hub device) still for about 6s when our product power cycle and reconnect. And It is particularly important to note that this phenomenon only occurs under the conditions mentioned above.
We capture the data of USB, and show error as below photo. Could you please help analyze it and provide some suggestions?