I found the MDI design requirement in the schematic checklist for DP83TC812S
1.termination resistor is recommended as 1kohm , 0.75W -> in the open alliance the power rate is 0.4W , I want to know which test requires the 1k resistor power rate?
2.DC blocking capacitors is recommended as 0.1uF 100V -> if there is ESD diode in the connector , if 50V is oK ?
3. ESD shunt resistor 100kohm -> it is used to absorb the ESD energy? how to decide the power value?
By the way what is the purpose of the CM termination ? I know it is the requirement of the open alliance.