This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TFP410-EP DE generator支持1080p, 720p问题

Other Parts Discussed in Thread: TFP410-EP, TFP410

各位专家好,

我们准备使用TFP410-EP显示1080p 和720p的视频,在查看数据手册的时候,发现如下问题:

1)TFP410-EP可使用内部DE generator来生成DE信号

2)DE generator的H_RES,V_RES有大小限制,<=2047

3)对1080p,对任意帧率,根据SMPTE-274M, H_RES>=2200

4)对720p,对于<=30帧的,H_RES>=3300

显然,使用内部DE generator,无法正常显示上面3),4)两种情况。

那么我们想请专家确认下面的问题:

1)不使用内部DE generator,外部提供DE信号,是否可以不受H_RES,V_RES大小的限制,正确显示上述3),4)情况的视频?

2)或者,即使使用外部DE信号,仍无法正确显示上述3),4)情况的视频?

3)否则,是否有你们的客户,已经使用TFP410-EP显示1080p的视频,或者720p30/24 ... 等低帧率的视频?(确认视频是完整正确的显示,而不是有剪切、或不完整显示的情况?)

盼专家回复,谢谢!