Other Parts Discussed in Thread: DS90UB953-Q1, , DS90UB953A-Q1
DS90UB954-Q1接收DS90UB953-Q1傳送過來的影像資料,會有破圖現象.
讀取DS90UB954-Q1暫存器,在開啟的時候,讀取0x4D會得到0x13,在破圖瞬間會得到0x33 [5] BCC_CRC_ERROR會報錯誤出來.
請問這問題該從哪裏著手確認硬體電路上哪裏有問題.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DS90UB954-Q1接收DS90UB953-Q1傳送過來的影像資料,會有破圖現象.
讀取DS90UB954-Q1暫存器,在開啟的時候,讀取0x4D會得到0x13,在破圖瞬間會得到0x33 [5] BCC_CRC_ERROR會報錯誤出來.
請問這問題該從哪裏著手確認硬體電路上哪裏有問題.

我有几个问题想更好地理解发生了什么:
1)有多少台摄像机连接到DES?
2)这里用的是什么SER?
SER和DES上配置了什么模式?
4)什么电缆类型和长度?
5)他们是否测试了一个以上的解串器板?
6)问题总是发生在相同的摄像机上吗?连接到同一块电路板上?
7)如果他们切换摄像机或用其他摄像机替换它们,问题是否仍然存在?
8)串行器以哪种时钟模式运行?
9)他们使用的是哪种图像传感器?以及传感器输出的是哪种数据类型/分辨率/帧率?
10)哪个犯罪现场调查CLK / PCLK将进入序列化程序?
11)从反串行化器出来的是什么样的CSI-CLK?
12)两端使用的是哪个外部时钟值?
13)如果可用,串行器侧的外部时钟是直接连接到传感器还是串行器?
14)我们以前做过任何原理图审查吗?
15)串行器输入端的数据/时钟有多好?
16)锁定信号是低、高还是切换?
17)他们有功能性I2C通信吗?本地和远程?
18)它们是否遵循数据手册中描述的两个器件的上电顺序?
Dear Sir,
1)有多少台摄像机连接到DES?answer:目前是1 chanel camera連接到DES.
2)这里用的是什么SER? answer:TI DS90UB953A-Q1
3)SER和DES上配置了什么模式?
4)什么电缆类型和长度?answer:Fakra RG174 Cable 1m
5)他们是否测试了一个以上的解串器板?answer:測試了約50PCS DES Board 約有10%這樣的問題.
6)问题总是发生在相同的摄像机上吗?连接到同一块电路板上? answer:用同一組SER Camera及同一組cable做傳輸 連接到不同的DES Board.
7)如果他们切换摄像机或用其他摄像机替换它们,问题是否仍然存在?answer:問題跟著DES Board發生.
8)串行器以哪种时钟模式运行?answer:TI953使用外部REFCLK(24MHz)供應給sensor。MIPI書出clock模式為continuous clock
9)他们使用的是哪种图像传感器?以及传感器输出的是哪种数据类型/分辨率/帧率?answer: OmniVision OS02H10 RAW10 1920x1080 30fps
10)哪个犯罪现场调查CLK / PCLK将进入序列化程序?answer:TI953提供24MHz REFCLK給sensor
11)从反串行化器出来的是什么样的CSI-CLK?answer:TI954輸出CSI clock: MIPI CSI-2 continuous clock, 812.5Mbps/lane
12)两端使用的是哪个外部时钟值?answer:SES透過DES外部振盪器提供.

13)如果可用,串行器侧的外部时钟是直接连接到传感器还是串行器?answer:如上圖,由SER提供給SENSOR
14)我们以前做过任何原理图审查吗?answer:有.
15)串行器输入端的数据/时钟有多好?answer:不太懂這意思?
16)锁定信号是低、高还是切换?answer:傳輸畫面訊號正常時,LOCK pin = High,訊號段開時,LOCK pin = LOW
17)他们有功能性I2C通信吗?本地和远程?answer:可以透過I2C存取
18)它们是否遵循数据手册中描述的两个器件的上电顺序? answer:有按照上電時序.
感谢您提供以上详细信息。
你能提供来自SER和DES的寄存器转储,来自一个好的工作系统和来自一个有故障的系统吗?
我最感兴趣的是这些寄存器:
UB953: 0x02-0x07,0x10-0x11,0x32,0x37,0x50-0x52,0x55,0x56,0x5B-0x64
UB954: 0x02-0x06,0x1F-0x24,0x33-0x37,0x40-0x49,0x4B-0x58,0x5B-0x6D,0x70-0x76,0x7A-0x7C,0xA5,0xD2-0xDB。
Dear Sir,
讀取出暫存器數值如下,分成良品(good)與不良品(bad).
UB953:
reg, data(good) | data(bad)
0x02, 0x53 | 0x53
0x03, 0x48 | 0x48
0x04, 0x00 | 0x00
0x05, 0x03 | 0x03
0x06, 0x41 | 0x41
0x07, 0x28 | 0x28
0x10, 0x00 | 0x00
0x11, 0x00 | 0x00
0x32, 0x09 | 0x09
0x37, 0x7A | 0x7A
0x50, 0x20 | 0x20
0x51, 0xC0 | 0xC0
0x52, 0x47 | 0x47
0x55, 0x01 | 0x01
0x56, 0x00 | 0x00
0x5B, 0x00 | 0x00
0x5C, 0x00 | 0x00
0x5D, 0x00 | 0x00
0x5E, 0x00 | 0x00
0x5F, 0x00 | 0x00
0x60, 0x00 | 0x00
0x61, 0x2B | 0x2B
0x62, 0x60 | 0x60
0x63, 0x09 | 0x09
0x64, 0x1D | 0x1D
UB954:
0x02, 0x1E | 0x1E
0x03, 0x20 | 0x20
0x04, 0xDB | 0xDB
0x05, 0x01 | 0x01
0x06, 0x00 | 0x00
0x1F, 0x00 | 0x00
0x20, 0x00 | 0x20
0x21, 0x01 | 0x01
0x22, 0x00 | 0x00
0x23, 0x00 | 0x00
0x24, 0x00 | 0x00
0x33, 0x03 | 0x03
0x34, 0x40 | 0x40
0x35, 0x01 | 0x01
0x36, 0x00 | 0x00
0x37, 0x00 | 0x03
0x40, 0x00 | 0x00
0x41, 0xA7 | 0xA7
0x42, 0x71 | 0x71
0x43, 0x01 | 0x01
0x44, 0x00 | 0x00
0x45, 0x00 | 0x00
0x46, 0x00 | 0x00
0x47, 0x00 | 0x00
0x48, 0x00 | 0x00
0x49, 0x00 | 0x00
0x4B, 0x12 | 0x12
0x4C, 0x12 | 0x12
0x4D, 0x40 | 0x40
0x4E, 0x02 | 0x02
0x4F, 0x00 | 0x00
0x50, 0x00 | 0x00
0x51, 0x00 | 0x00
0x52, 0x00 | 0x00
0x53, 0x00 | 0x00
0x54, 0x00 | 0x00
0x55, 0x00 | 0x00
0x56, 0x00 | 0x00
0x57, 0x00 | 0x00
0x58, 0x5E | 0x5E
0x5B, 0x00 | 0x00
0x5C, 0x30 | 0x30
0x5D, 0x78 | 0x78
0x5E, 0x00 | 0x00
0x5F, 0x00 | 0x00
0x60, 0x00 | 0x00
0x61, 0x00 | 0x00
0x62, 0x00 | 0x00
0x63, 0x00 | 0x00
0x64, 0x00 | 0x00
0x65, 0x78 | 0x78
0x66, 0x00 | 0x00
0x67, 0x00 | 0x00
0x68, 0x00 | 0x00
0x69, 0x00 | 0x00
0x6A, 0x00 | 0x00
0x6B, 0x00 | 0x00
0x6C, 0x00 | 0x00
0x6D, 0x7C | 0x7C
0x70, 0x6B | 0x6B
0x71, 0x6B | 0x6B
0x72, 0xFE | 0xFE
0x73, 0x00 | 0x00
0x74, 0x00 | 0x00
0x75, 0x00 | 0x00
0x76, 0x00 | 0x00
0x7A, 0x00 | 0x00
0x7B, 0x00 | 0x00
0x7C, 0x20 | 0x20
0xA5, 0x19 | 0x19
0xD2, 0x94 | 0x94
0xD3, 0x04 | 0x3F/0x17/0x05/0x04/0x2F/0x37
0xD4, 0x60 | 0x60
0xD5, 0xF2 | 0xF2
0xD6, 0x00 | 0x00
0xD7, 0x03 | 0x01/0x00/0x03
0xD8, 0x00 | 0x00
0xD9, 0x00 | 0x00
0xDA, 0x00 | 0x00
0xDB, 0x00 | 0x00
你的转储有问题。在两个器件上,我可以看到没有锁定(见DES寄存器0x04[2=0]),这意味着SER和DES之间没有通信。此外,没有接收到任何数据(见DES寄存器0x73-0x76 all = 0)。
请仔细检查您的设置并提供正确的转储。
There is something wrong with your dumps. On both devices I can see there is no LOCK (see DES reg 0x04[2=0]), which means no communication between SER and DES. Also, there is no any received data (see DES reg 0x73-0x76 all = 0).
Please double check your setup and provided correct dumps.