DP83TD510E-EVM: How to configure RMII repeater mode

Part Number: DP83TD510E-EVM
Other Parts Discussed in Thread: DP83TD510E

Hello, I would like to inquire about the usage of DP83TD510E The problem is as follows:
I hope to configure both DP83TD510E in repeater mode to achieve back-to-back communication,
I have configured the pins to repeater mode according to the first picture, and also pulled up the RX-D2 (pin14) pin according to the second picture,
May I ask if this is the correct repeater mode? Can two PHY communicate with each other?
When I tried to pull up the RX-D2 (pin14) pin, I found that the pin was not pulled up successfully. I ensured that my power supply was normal, and I measured the pin voltage with an oscilloscope to be around 0.5V, but it was not pulled up successfully. May I ask why this is? Will this phenomenon cause problems with my configuration?aa.jpgbbb.jpg