THVD1452DGSR芯片DE与RE引脚连到一起后与单片机GPIO引脚PA10直连,PA10输出低电平时(推挽或者下拉),芯片的DE引脚会有1.5V的电压值(此时没有下拉电阻),在DE和RE引脚加入下拉电阻后会有2.7V的电压值
您好,
THVD1452是Full-Duplex器件,RE脚在芯片内部有2M的上拉电阻,DE引脚在芯片内部有2M的下拉电阻。
如果将RE和DE直连,请确认电阻匹配,通常10K的下拉是可以的(数据手册 Figure 37)。
Mitigating UART Receiver Glitches While Switching Modes on RS-485 Transceivers