Other Parts Discussed in Thread: ISOW1412
Hi,请教一个问题。
在应用中,2个系统使用485进行通讯。一侧使用SN65176BDR,5V供电,输出有120Ω终端电阻,SN65176BDR的485A使用电阻上拉到5V,485B使用电阻下拉到GND。另一侧使用ISOW1412,输出选择电压为5V_iso,它的485A和485B均使用电阻下拉到它隔离电源的地GND_iso。双绞线长度2m。接线图如下图所示。
测试结果如下图,CH3为SN65176BDR的DE信号,CH4为485BUS。SN65176BDR的输出电平为±4.3V,而ISOW1412的电平为±5V。请问造成电平不一致的原因是什么?应该如何应对?