This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65CML100: SN65CML100

Part Number: SN65CML100
Other Parts Discussed in Thread: SN65LVDS100

1.在SN65CML100规格书中没有差分引脚短路电流Ios的值,能否给出该值,下图为其他芯片的示例。我们需要确认在out-/out+引脚短接到地或者短接到+3.6V,器件会不会损坏。尤其当out引脚输出低时,外部+3.6V短接到引脚电流会是多少?器件会不会损坏?

image.png

2.对于SN65LVDS100,同样是输出引脚短路电流,只写了接到地的电流,如果接到VDD是否也可以保证不被损坏,-24mA和24mA是否代表了进入或从引脚输出的电流都被限制在24mA以内?

image.png

  • 您好,收到了您的案例,调查需要些时间,感您的耐心等待。

  • 对地短路电流是任何LVDS驱动器最坏情况下的短路电流。虽然我们在部分此类器件的规格书中未明确说明对电源(VDD)的短路电流,但只要所施加的电压仍在推荐工作条件范围内,该电流值就不会超过对地短路的规格指标。
    CML采用开漏差分输出结构,其电流从外部电源端汲取。器件本身并不提供输出电流,因此若这些引脚未连接任何外部线路且被短路至地,电流将为零。