This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL16C754C: INTSEL pin definitions (or wiring methods) for both TTL16C754C AND TL16C754BPN.

Part Number: TL16C754C

INTSEL pin definitions (or wiring methods) for both TTL16C754C AND TL16C754BPN.

針對TL16C754C與TL16C754BPN.兩者的INTSEL接腳定義(或接法)  兩者的INTSEL接腳定義

My original question was whether INTSEL meant either floating or not connected. However, I discovered that the new process version of the TL16C754C (64-pin) doesn't have an INTSEL pin at all; instead, the INTSEL function is indicated in the model number. Specifically, the INTSEL pin in the TL16CP754C is directly connected to HIGH, while the INTSEL pin in the TL16CM754C is directly connected to LOW.

Therefore, my original question was why TI only lists the TL16CP754C and not the TL16CM754C?

我原先要問的是INTSEL是不是就是floating或不接 後來發現新製程的TL16C754C 64腳版本根本沒有INTSEL接腳 而將INTSEL的功能表示在型號裡面 即TL16CP754C內的INTSEL接腳直接接HIGH 而TL16CM754C內的INTSEL接腳直接接LOW 
因此我原來的問題是為什麼TI只查得到TL16CP754C 查不到TL16CM754C ?