This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MN34229+SN65LVDS324 帧大小错误 ,请教高手!

MN34229+SN65LVDS324,MN34229驱动中设置有效像素宽1944,高1092,2CH-2PORT,1080P60模式,

设置SN65LVDS324寄存器配置:

0x09---0x02,

0x0a---0x62,

0x0b---0x07,

0x0c---0x98,

0x0d---0x04,

0x0e---0x44,

配置完后读取寄存器为:

0x09---0x02,

0x0a---0xe2,

0x0b---0x07,

0x0c---0x98,

0x0d---0x04,

0x0e---0x44,

0x10---0x00,

0x11---0x80,

此时图像显示正常,然而0x11为何一直为0x80,这个位表示图像帧大小错误,我修改了不同的0x0b、0x0c、0x0d、0x0e的值,但是一直都无法消除该错误,请问该如何设置可以消除该错误状态?虽然图像出来了,但是在某些状态下会出现异常,对这个错误状态会引发什么问题不清楚,所以还是要解决这个帧大小报错的问题,谢谢!

  • 我问下产品线,看有没有建议。

  • 产品线的回复:

    please let me know both the frame of active video and the blanking. if you are sending 1080p active video, please try to configure default in LVDS324.

  • 你好,我在使用IMX185时也碰到这个问题,在IMX185中有很清楚的图像区域设置,我把这种模式的图发上来,现在IMX185使用的是LVDS PARALLEL 输出模式,1080P60 12bit,水平方向像素(HMAX)2200,水平方向像素(VMAX)1125,像素及录区:1920*1080,我按照IMX185的图上说的1952*1115,1945*1105,1937*1097,1920*1080,这些组合均设置到LVDS324的0xB、0xC、0xD、0xE寄存器中,读取0x11寄存器却为0x88,这个问题一直无法解决,LVDS324端怎样才能设置到正确的值呢,或者能检测到输入的数据的有效像素区域大小?