Part Number: TXS0206A
我准备用TXS0206A做SD3.0接口的电平转换。
我的SD HOST的IO接VCCA,SD SLAVE的IO接VCCB。
SD SLAVE侧的电平是固定的1.8V,所以我直接接1.8V即可。
但根据SD3.0的协议,HOST端的IO初始的是3.3V,然后切换成1.8V。
1、这个状态下,我的VCCA应该怎么接多少V的电源?
2、如果直接接1.8V电源,当初始IO为3.3V的时候会不会有问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个不是VCCA应该怎么接的问题,是这款芯片不支持SD 3.0这个应用。
https://e2e.ti.com/support/logic-group/logic/f/logic-forum/929386/txs0206a-sd3-0-support
我们也帮您看了目前TI现有的接口芯片,我们目前尚无针对SD3.0电平转换的解决方案。