This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Level的等级是根据EQ GAIN不同来划分的等级,从8.2.3部分的眼图来看,level 2的EQ gain最大,level3的EQ Gain最小
VREG只有在高速模式下才会启动,或者说TUSB211只对高速信号进行均衡。
高速模式不是硬件启动的,是由主机发送一个USB 高速test packet,按照datasheet中的步骤之后HS就启动了
Connect USB test fixture (Terminated at scope)
Configure desired EQ setting on TUSB211.
Power on TUSB211 (With Test fixture connected).
Start sending test packet .
只有1.5m的延长线,放一个TUSB211就够了,如果cable线很长的话,可能需要多个TUSB211进行redriver。
Hi, Kailyn.
想要請教一下這顆料件,他的spc有一段說明如下
USB High Speed boost select via external pull down resistor. Sampled upon power up.
Auto selects min EQ when left floating. Does not recognize real time adjustments
在pin descreption那一頁,這是不是就是說,這隻腳如果我浮接的話,他會自動根據衰弱的多少來自動補償。
這樣理解是否有問題。
如果是這樣的話,那這顆電阻是否可以不用上。不上的話可能會有什麼問題。
因為我們是想要放在cable內, cable的長度為2/3/5米,長度不一定。訊號品質可能也會不同。
我原來的想法是設定成最大EQ。